Firestop Goes BIM

Introducing the Hilti Button for Firestop

Plano, TX. – June 6, 2016 — The new Hilti Button for Firestop is the first firestop automation software to integrate with building information model (BIM) software platforms. The Hilti Button automates the firestop product and UL system selection process and eliminates the tedious, time consuming and manual task of placing hundreds of firestop objects in BIM. What used to take hours of a designer’s time, can now be done with the Hilti Button in just a click.

The Hilti Button automatically detects penetrations in fire-related construction and populates the appropriate firestop products and UL systems directly into BIM to save time, increase efficiency and reduce costs. Incorporating the Hilti Button for Firestop with BIM will improve quality control and help with coordinating schedules.

By seamlessly integrating with the Autodesk ecosystem around Navisworks Manage, AutoCAD, Fabrication CADmep, and Revit, the Hilti Button automates the firestop selection process on a project. Using attributes in the BIM model for clash detection, the Hilti Button identifies penetrations going through fire rated barriers that need to be firestopped. That information from clash detection is then pulled into Firestop Manager. This automatic process reduces the number of hours spent on the jobsite and in the office by manually identifying which penetrations need to be firestopped.

After the penetrations needing firestop are identified, the Hilti Button automates the firestop product and UL system selection process by identifying an appropriate firestop product and UL system for penetrations based on the attributes in the model. This helps to eliminate the need for plans and codes to be reviewed by firestop experts for specific products and systems on a project. After reviewing and/or updating the firestop product and UL system selection, the user can generate comprehensive submittal documents, create a Bill of Material and place direct orders via Hilti online.

For more information about the Hilti Button for Firestop, please contact Hilti Customer Service. From the U.S., call Hilti, Inc., at 1-800-879-8000 or visit www.us.hilti.com; from Canada, call Hilti (Canada) Corporation at 1-800-363-4458 or visit www.hilti.ca. 

About Hilti, Inc.

Hilti is a world-leading manufacturer and supplier of quality, innovative and specialized tools and fastening systems for the professional user. With more than 1,500 highly trained Hilti account managers and engineers throughout North America and an additional 1,300 Hilti employees nationwide, Hilti expertise covers the areas of powder actuated fasteningdrilling and demolition, cordless power tools, diamond coring and cuttingmeasuring toolsfirestopping, screw fastening, adhesive and mechanical anchoring, and strut and hanger systems.

Share

CONTACT US
CONTACT US