Added to cart
Added to cart
Go to shopping cart

Hilti Firestop Cast-in Devices CFS CID

The industry’s first firestop solution for 8" and 10" pipe

CFS CID drop in firestop device

Plano, Texas – July 17, 2017 — Hilti is making fire protection easier with the introduction of the new firestop cast-in devices CFS CID — the first and only cast-in devices for 8" and 10" pipes for water drainage and large pipe applications. These new one-step firestop solutions work with 8" PVC, metal pipes with insulation, as well as 8" and 10" metal pipes — no additional sealing is required. Hilti CFS CID firestop devices are available in 6", 8", 10", 12" and 14" heights.

Unlike traditional methods, Hilti’s CFS-CID 8" and 10" devices require only one laborer for installation, increasing job site productivity and reducing labor costs. The cast-in devices are ready to use right out of the package and installation process is simple, which helps lessen the chance of project delays caused by failed inspections.

Hilti CFS-CID 8" and 10" firestop cast-in devices are suited for new building construction, work with PVC, metal and metal with insulation pipes, and they do not have an expiration date (no shelf life).

With this solution, Hilti continues to have the most complete portfolio of products and services for mechanical trade firestopping.

For more information about Hilti CFS-CID 8" and 10" firestop cast-in devices, please contact Hilti Customer Service. From the U.S., call Hilti, Inc., at 1-800-879-8000 or visit www.hilti.com; from Canada, call Hilti (Canada) Corporation at 1-800-363-4458 or visit www.hilti.ca.

*Some limitations apply. Contact Hilti for details.

About Hilti, Inc.

Hilti is a world-leading manufacturer and supplier of quality, innovative and specialized tools and fastening systems for the professional user. With more than 1,700 highly trained Hilti account managers and engineers throughout North America and an additional 1,300 Hilti employees nationwide, Hilti expertise covers the areas of powder actuated fastening, drilling and demolition, cordless, diamond coring and cutting, measuring, firestopping, screw fastening, adhesive and mechanical anchoring, and strut and hanger systems.

Share

CONTACT US
CONTACT US