Update of quantity
Please note, the order volume has been updated. This is due to package and minimum order quantities.
Please note, the order volume has been updated to. This is due to package and minimum order quantities.
Plano, Texas – Oct. 20, 2017 – Digitize the entire measuring process with the new Hilti laser range meter PD-CS. Using an integrated laser module to capture and save measurements data directly onto photographs taken by its internal digital camera, the Hilti laser range meter PD-CS will help make contractors and site supervisors more productive, and eliminate the need for multiple devices — including paper and pencils.
The Hilti PD-CS allows the user to measure distances to 656 ft (200 m) with an accuracy of +/- .04-inch (1 mm) and add context to store data with pictures and/or text. Collected information can then be shared in a single PDF report or spreadsheet (CVS) using Bluetooth, Wi-Fi or a Micro USB connection.
The two 5 MP cameras with zooming capabilities on the Hilti PD-CS make locating a target outdoors or at long distances very easy. The user can take direct and indirect measurements and calculate area and volume among many other applications. Notes can easily be added to measurements and photos, and users can create project folders for different jobsites.
The Hilti PD-CS uses an Android based technology and has a color touch screen that is usable even with work gloves on. It has 8 GB of memory and will store more than 6000 measurements with photos. The unit has an integrated Li-Ion battery with a 10-hour battery life.
Also, the new Hilti laser range meter PD-CS is covered by the Hilti Tool Warranty 20/2/1 — 20 years of repair or replacement of defective parts; 2 years no cost repair including wear and tear; and a guaranteed 1-day turnaround on repairs. *
For more information about the Hilti PD-CS, please contact Hilti Customer Service. From the U.S., call Hilti, Inc., at 1-800-879-8000 or visit www.hilti.com; from Canada, call Hilti (Canada) Corporation at 1-800-363-4458 or visit www.hilti.ca.
*Some limitations apply. Contact Hilti for details.
Hilti is a world-leading manufacturer and supplier of quality, innovative and specialized tools and fastening systems for the professional user. With more than 1,700 highly trained Hilti account managers and engineers throughout North America and an additional 1,300 Hilti employees nationwide, Hilti expertise covers the areas of powder actuated fastening, drilling and demolition, cordless, diamond coring and cutting, measuring, firestopping, screw fastening, adhesive and mechanical anchoring, and strut and hanger systems.
Learn more
Share
To see account specific prices and content, please choose appropriate account.