Laser Range Meter PD-C

Plano, TX. – Messy paper trails can really slow you down, especially when you have a lot of jobsite areas to visit. The new Hilti Laser range meter PD-C is here to help. The PD-C captures and saves measurement data directly onto digital photographs taken by an integrated camera and laser module. Users can document jobsites, add comments, and export data into a single report. Digitize the entire measurement process from capturing measurements, to adding context to these measurements, and finally connecting your device and sharing this valuable data – all with one easy-to-use tool.

Capture

Thanks to the PD-C’s camera targeting function, contractors can spot the laser target easily whether indoors or outdoors, under any light condition. Leave guess-work behind with the PD-C’s time-saving intuitive guides and geometric calculations built into the software and easily visible on the large smartphone-like screen. Smooth navigation and a strong Gorilla® Glass display ensures the PD-C is ready for use on any jobsite.

Context

The PD-C features 4GB of memory and can store over 3000 measurements with pictures. Simply point, shoot and mark dimensions directly onto the photo. One person is able to accurately measure heights to ceiling and long distances up to 656 ft. The PD-C makes it easy to document where and what you measured so you can report issues, plan material orders, or collaborate more effectively.

Connect

Share project data in a single PDF or CVS report and transfer it conveniently via USB to any computer, or Bluetooth to Android devices. Photos with measurements can be exported as a JPG file. A clear digital document trail makes it easy to generate accurate estimates to help insure that the right amount of materials are purchased, or verify that work is completed to specification.

Hilti lasers are dedicated to precision accuracy yet even with built-in protection features, such instruments can be affected over time by everyday use. The PD-C is covered by Hilti’s Tool Warranty 20/2/1 which consists of 20 years of repair or replacement of defective parts; 2 year no cost repair including wear and tear; and a guaranteed 1-day in-and-out of our Repair Center on repairs.* The PD-C is also backed by Hilti Calibration Service to provide reliability and accuracy. The PD-C will be calibrated, and adjusted if needed, with the calibration confirmed in writing for professional assurance.

For more information on the Hilti laser distance measurers or the Laser range meter PD-C, please contact Hilti Customer Service. From the U.S., call Hilti, Inc., at 1-800-879-8000 or visit www.us.hilti.com; from Canada, call Hilti (Canada) Corporation at 1-800-363-4458 or visit www.hilti.ca.

*Some limitations apply. Contact Hilti for details.

About Hilti, Inc.

Hilti is a world-leading manufacturer and supplier of quality, innovative and specialized tools and fastening systems for the professional user. With more than 1,500 highly trained Hilti account managers and engineers throughout North America and an additional 1,300 Hilti employees nationwide, Hilti expertise covers the areas of powder actuated fasteningdrilling and demolition, cordless power tools, diamond coring and cuttingmeasuring toolsfirestopping, screw fastening, adhesive and mechanical anchoring, and strut and hanger systems.

Share