Firestop solutions for pipe penetrations

We offer firestop solutions for all common piping applications including heating, plumbing, air conditioning and cooling systems

Public awareness of fire safety in buildings has surged. Building owners and occupants alike are now demanding passive fire protection – that is, features within the structure to help prevent flames, heat and smoke from spreading – which can help save lives and minimize damage if fire breaks out. Pipe penetration assemblies are critical areas for firestopping. Even these seemingly small gaps in fire-rated walls and floors are enough for smoke and toxic gasses to spread through. To maintain the fire resistance of walls and floors, it is essential that every opening is sealed using a well-designed and installed firestop system.

Despite its undeniable importance, firestopping is still often treated as an afterthought. Cost overruns, strained budgets and scheduling conflicts between trades on-site are virtually unavoidable if fire protection is neglected until the final project phases.

Loading

Labor-saving, one-step, cast-in firestop solutions

Firestop cast-in device

The CP 680/CFS-CID (cast-in device) is a game-changer for firestopping pipe floor penetrations. It is a one-step, cast-in solution for both plastic and metal pipes – a productivity booster, a true space saver and easier to inspect. By planning and specifying cast-in devices before casting the slabs, firestop is shifted from the last step to the first. No coring and drilling are required, and on-site trade coordination becomes much simpler. The integrated smoke gasket in the device makes caulking unnecessary.  

The firestop performance of pre-formed devices doesn’t rely on the installer’s skills. The risk of failed inspections due to faulty installation is therefore significantly reduced.

The systems are available for both flat concrete and composite metal deck slabs.

Learn more about firestop cast-in devices

Simpler firestop inspections

With so much choice out there, how can you be sure that you have chosen the right firestop solution to comply with regulations and pass inspections? When you work with Hilti to specify firestop for pipe penetrations, our firestop experts support you from design, installation, and inspection to documentation. You enjoy the model code compliance, budget, and penetration types that have been matched with the correct firestop solution.

In addition, you can use digital tools to speed-up design and documentation. Our online firestop product selector, based on an extensive UL-approved products database, simplifies product selection and helps with model code compliance. The PC-based Documentation Manager is a highly efficient method for automating firestop documentation.

Learn more about Documentation Manager

Related products

  • Hilti firestop sealant FS-ONE MAX

    Firestop sealants

    For plastic and metal pipes

    Show me more
    Hilti firestop Cast-in Device CP 680

    Firestop cast-in and drop-in devices

    For plastic and metal pipes in floor applications

    Show me more
    Hilti firestop collars CFS-C P

    Firestop collar devices

    Designed to form a barrier for combustible plastic pipe penetrators

    Show me more
    Hilti firestop foam CP 660

    Firestop foam

    Designed for small to medium sized openings

    Show me more

Share