Self-leveling Lasers

Self-leveling lasers beat manual alignment, automatically

Of all the things that challenge the pursuit of perfection on your job site, nothing is more frustrating than depending on a tool that is out of alignment. Fortunately, that is one possibility Hilti self-leveling lasers can help you cross off your already-too-long list of concerns.

The auto-leveling feature in our self-leveling lasers is based on an internal pendulum to better ensure that you can establish and maintain level lines over long distances. That can be up to 66 feet when used alone or nearly 100 feet when matched with a Hilti laser receiver. Plus, after a not-so-rare occurrence of accidental displacement, this same feature automatically brings your laser line or point back into level.

Two beam line lasers

PM 2-L

Red beam line laser with 2 lines for leveling, aligning, and squaring

Shop now for the PM 2-L

PM 2-LG

Green beam line laser with 2 lines for leveling, aligning, and squaring

Shop now for the PM 2-LG

PMC 46

Red beam combi-laser with 2 lines and 4 points for plumbing, leveling, aligning, and squaring.

Shop now for the PMC 46

Multi-line lasers

PM 4-M

Red beam multi-line laser with 3 lines and plumbing point.

Shop now for the PM 4-M

PM 40-MG

Green beam multi-ligne laser with 4 lines for plumbing, leveling, aligning, and squaring.

Shop now for the PM 40-MG

Rotating Lasers

PR 3-HVSG

  • Leveling - suspended ceilings, transferring heights
  • Squaring - walls, partitions
  • Aligning - pipe runs and cable trays
Shop now for the PR 3-HVSG

PR 30-HVSG A12

  • Leveling – suspended ceilings, raised floors, transferring heights
  • Squaring – partition walls
  • Aligning – drywall, pipe runs, cable trays etc.
  • Grading – inclined interior ceilings, hand rails, pipes etc.
Shop now for the PR 30-HVSG A12

Your Hilti Tool Warranty—Warranty Redefined

All our laser measure and detection systems tools are supported by the Hilti Tool Warranty.

  • For the first 20 years, we will repair or replace parts that break from defects in materials or workmanship.
  • For the first two years from date of purchase, we provide wear-and-tear coverage at no cost.
  • We guarantee to have every tool repair in and out of our repair center in one day or the repair is free.
  • On top of all that, every Hilti laser measure tool comes with one free calibration per year for your first two years of ownership.

*Some exceptions apply. See the Hilti Tool Warranty page for details.

 

 

Share