Water can’t be controlled on the jobsite, but you don’t have to lose control in design
The moisture condition of concrete has been defined by ACI 318-19 Chapter 26 as a key parameter that needs to be considered during the design and specification of adhesive anchors. Dry concrete, water-saturated concrete, and water-filled holes may have different strength reduction factors which can impact the bond strength of the adhesive and may cause jobsite issues if not accounted for in the design process. - Webinar
sessions
|
0.5 Hilti PDH


1 séance à venir
September 8th, 2026 / 11:00 AM (CDT)
Instructeur: Abraham Chapa
Hilti Hilti PDH: 0.5
Inscription fermée
Matériel de présentation
Télécharger