Skip to main content

Require Engineering Judgment for fire stopping of a gap above a elevator door frame

Posted by Amir Badriabout 2 years ago
Require Engineering Judgment for fire stopping of a gap above a elevator door frame

We require an engineering Judgment for using fire stopping for the below existing condition of the gap above an elevator door frame at a Hotel building:

As you can see in the attached SK-7 & SK-9, above the stainless steel elevator door frame at the left side where the 5/8" dry walls are connected to the stainless steel elevator door frame and the existing concrete blocks, there is a less than 5/8" gap which is filled with concrete grout. For this area, please provide a ULC design number and fire-stopping product from Hilti which would be code compliant and practical for this specific scenario.

In advance, thanks for your time and assistance.

Best Regards,
Amir Badri, MASc, M.Eng.
Designer
CDCD Engineering Limited
303 Cedar Street
Sudbury, ON
P3B 1M8
Ph: 705-674-8457, Ext. 8#
Fax: 705-674-7839
Email: amir.badri@cdcdengineering.com

fire,Engineering,Judgment,stopping,elevator

1 Reply
Posted by GHINA KABBARAabout 2 years ago
Hilti Verified

Hi Amir,
Kindly submit an Engineering Judgement Request through the Hilti Construction Platform on the link below:
https://hcp.hilti.com

EJ