Update
Please note, the order volume has been updated. This is due to package and minimum order quantities.
Please note, the order volume has been updated to. This is due to package and minimum order quantities.
Please note, the order volume has been updated. This is due to package and minimum order quantities.
Please note, the order volume has been updated to. This is due to package and minimum order quantities.
What can we build that’s better? Stronger? Safer? Since 1941, the name Hilti has been synonymous with innovation. Everything we do helps build better futures—and that includes the future of the construction industry.
Every day at our research, development and testing centers in Europe, North America and Asia, Hilti engineers and experts are tinkering, testing and imagining new ways to make your work easier, safer and more productive. We work directly with customers about the challenges they face and work to solve them with better, smarter products. We work with various universities and independent research laboratories to tackle the most challenging technical problems. In other words, we never stop improving—because you never stop working.
The jobsite—where installer experience can vary dramatically—is no place to experiment with anchors.
That’s why we thoroughly test and document the performance parameters and application and installation guidelines for every Hilti anchor. It’s also why we offer fastening systems design software to help automate the process of finalizing your choice with confidence.
But we’re not the only ones to document Hilti performance. Our nearly 300 pieces of anchor documentation include specifications and approvals from International Code Council-Evaluation Service (ICC-ES), UL, Certificate of Label Approval, NSF LEED and other industry-recognized organizations.
If you have questions about past anchoring problems or installation concerns for upcoming applications, connect with our Customer Service team for one-on-one guidance.
ICC-ES Acceptance Criteria AC308 for Post-Installed Adhesive Anchors
ICC-ES Acceptance Criteria AC193 for Mechanical Anchors
HIlti tests to these criteria include:
For masonry applications, we adhere to the following test standards:
Whether your biggest concern is withstanding a potential fire emergency years down the road—or simply complying with current construction codes regarding firestop installation—Hilti offers multiple products and resources to foster confidence.
Our in-house lab conducts firestop testing in accordance with ASTM E814 / UL 1479 for through-penetration firestop systems and ASTM E1966 / UL 2079 for construction-joint firestop systems. That means you can trust the F-rating and T-rating for each Hilti firestop system assembly. Optional tests are also frequently conducted to determine air leakage ratings (L-rating])and water leakage ratings (W-rating) of a firestop system assembly to ensure they meet your requirements.
Gain insight into the performance of various styles of Hilti mechanical deck fasteners for your applications with deck fastener testing that covers small element connection tests used to determine fastener pullout, pullover, and lap-joint shear strength and stiffness.
The results generated by these deck fastener testing steps can be analyzed and used as a predictive model to calculate performance of larger steel deck diaphragm assemblies or systems.
For your confidence, this deck fastener testing is conducted in accordance with the following industry-accepted standards:
Full-scale diaphragm system tests evaluate the performance characteristics of deck fasteners in an entire integrated steel deck diaphragm assembly. You can use the resulting data in predictive modeling that addresses varying configurations of base steel, steel deck, spans, and specific fastener combination options for your applications.
These tests are conducted in accordance with the following standards:
Uncompromise with Nuron Experience the latest cordless innovation. Discover Nuron
Our executive will call you back shortly
An e-mail has been sent to our Customer Service team for follow-up. You will receive a copy of your request for your records.
To see account specific prices and content, please choose the appropriate account.
Hilti = registered trademark of Hilti Corporation, 9494 Schaan, Liechtenstein © 2009-2016, Right of technical and programme changes reserved, S.E. & O
Our executive will call you back shortly
An e-mail has been sent to our Customer Service team for follow-up. You will receive a copy of your request for your records.