Passer au contenu principal

2020 National Building Code of Canada Firestop Requirements (FS330) - Webinar

Gain an overview of the firestopping guidelines used in the 2020 National Building Code of Canada

The National Building Code of Canada, and the Provincial codes, which are all based on the NBCC, include requirements for firestopping that are often perceived as confusing. This is partly due to the fact that the requirements are distributed across multiple sections of the code, rather than in one dedicated section. This webinar will help provide a clear overview of the code’s requirements for firestopping of penetrations, joints and curtain wall gaps, including the somewhat complex and not always consistent exceptions and variations. - Webinar


 sessions
|
1.5 Hilti PDH

Désolé, aucun résultat trouvé.

Matériel de présentation
2020 National Building Code of Canada Firestop Requirements (FS330) - Webinar
Télécharger