Passer au contenu principal

NBCC Requirements Related to Firestopping 2015 / 2020 (FS330-Canada) - Seminar

The National Building Code of Canada, and the Provincial codes, which are all based on the NBCC, include requirements for firestopping that are often perceived as confusing. This is partly due to the fact that the requirements are distributed across multiple sections of the code, rather than in one dedicated section. This webinar will help provide a clear overview of the code’s requirements for firestopping of penetrations, joints and curtain wall gaps, including the somewhat complex and not always consistent exceptions and variations. - Seminar


 sessions
|
1 Hilti PDH

Désolé, aucun résultat trouvé.